Other Parts Discussed in Thread: MSP430F5528
All:
Recently, I was asked to update from an older IAR Workbench to the newest. I am able to create a project and transfer the project settings, and even download and run the newly build project. The RAM size of the new project is very close to the one built with IAR 5.51 - however, when I looked at the amount of code being put into flash, the size went from ~20000 to ~28000 bytes. I am exploring why this happened, but I would like to know if someone else has seen this size increase.
I am using MSP430F5528.
Perplexed...