I am running CCS v4 Core Edition. When I want "Debuging", I get: "Error Initializing emulator: No USB FET was found". My emulator is MSP430 USB - Debug - Interface MSP - FET430UIF und I can see that is properly installed. My emulator with IAR works!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am running CCS v4 Core Edition. When I want "Debuging", I get: "Error Initializing emulator: No USB FET was found". My emulator is MSP430 USB - Debug - Interface MSP - FET430UIF und I can see that is properly installed. My emulator with IAR works!
Hi Admir,
What version of IAR are you using that it works with?
CCSv4 is a very old version - and it was before we changed to MSP430DLLv3 for the emulator firmware. Can you please go to device manager, and see if your MSP-FET430UIF is listed as CDC or VCP? CCSv4 will only support MSP430DLLv2, which will mean the MSP-FET430UIF would have to enumerate as VCP. If it says CDC, that means that the FET tool has MSP430DLLv3 firmware in it, and it will not be able to be recognized by any version of CCS older than CCSv5.1 or IAR EW 5.40.
My guess is that you have a newer IAR that uses DLLv3, and this is why your tool is recognized by your newer IAR but not by your older CCS.
The solution in this case would be to either download the latest version of CCSv6 (which has A LOT of improvements over CCSv4), or you will have to use your IAR to do a DLL downgrade when you want to switch between IDEs, and upgrade back when you want to use IAR again. I think the best recommendation would be to download the updated CCS version if you need to use CCS instead of IAR.
Regards,
Katie
Hi Admir,
I have IAR version 6.20.1 as well, so I tried to reproduce your issue, but I had no issue. Here is what I did:
Does this differ much from what you did? I was not able to recreate the issue with IAR 6.20.1.
What file is the #error directive in - does it point to a file or line of code somewhere?
Regards,
Katie
**Attention** This is a public forum