Other Parts Discussed in Thread: ENERGIA
Hello,
I am trying to read from a 9 Degrees of Freedom board using I2C on the f5529. I wanted to start off by using Energia library functions to test but for some reason, my program gets stuck during "Wire.endTransmission()". Any ideas on what is causing this? I have what code is written here so far, and I highlighted the line that's giving me trouble.
Thanks
#include <Wire.h>
#define ITG3200_ADDRESS (0xD0 >> 1)
//request burst of 6 bytes from this address
#define ITG3200_REGISTER_XMSB (0x1D)
#define ITG3200_REGISTER_DLPF_FS (0x16)
#define ITG3200_FULLSCALE (0x03 << 3)
#define ITG3200_42HZ (0x03)
int accelerometer_data[3];
int gyro_data[3];
int magnetometer_data[3];
int angle[3];
void i2c_write(int address, byte reg, byte data){
// Send output register address
Wire.beginTransmission(address);
Wire.write(reg);
Wire.write(data);
Wire.endTransmission();
digitalWrite(RED_LED, HIGH);
}
void i2c_read(int address, byte reg, int count, byte* data){
int i = 0;
//Send input register address
Wire.beginTransmission(address);
Wire.write(reg);
Wire.endTransmission();
//Connect to device and request bytes
Wire.beginTransmission(address);
Wire.requestFrom(address, count);
while(Wire.available()){ //slave may send less than requested
char c = Wire.read(); //receive a byte as character
data[i] = c;
i++;
}
Wire.endTransmission();
}
void init_itg3200(){
byte data = 0;
//Set DLPF to 42 Hz and set the scale to "Full Scale"
i2c_write(ITG3200_ADDRESS, ITG3200_REGISTER_DLPF_FS, ITG3200_FULLSCALE | ITG3200_42HZ);
//Make sure the register value is correct.
i2c_read(ITG3200_ADDRESS, ITG3200_REGISTER_DLPF_FS, 1, &data);
Serial.print((byte)data);
}
void read_itg3200(){
byte bytes[6];
memset(bytes,0,6);
//read 6 byres from the ITG3200
i2c_read(ITG3200_ADDRESS, ITG3200_REGISTER_XMSB, 6, bytes);
for (int i = 0; i < 3; i++){
gyro_data[i] = (int)bytes[2*i + 1] + (((int)bytes[2*i]) << 8);
}
}
void setup(){
Wire.begin();
pinMode(RED_LED, OUTPUT);
Serial.begin(9600);
Serial.print("begin\n");
digitalWrite(RED_LED, LOW);
for(int i = 0; i < 3; i++){
accelerometer_data[i] = gyro_data[i] = magnetometer_data[i] = 0;
angle[i] = 0;
}
init_itg3200();
}
void loop(){
Serial.print(ITG3200_ADDRESS);
Serial.print("\n");
//delay(100);
}