Hi,
I have developed a program and I successfully used MSP-FET debugger to debug the code.
Now I have to flash the Microcontroller but i am unsure with the methods. I tried following and seems like none worked.
1. As per refered in someother thread on E2E I enable the Hex Utility under properties. I also selected "Output TI-TXT hex format". But after running "Build" I still do not see any txt file generated in the Debug folder. I tried Intel hex form as well.
2. Which format do I need to select for MSP430?
3. What setting am I missing which prohibit hex file generation?
4. I also see there is link to Third party vendor software to flash the MSP430 But from the website the debugger is different. Will MSP-FET worj with the FET-Pro430 Lite software?
I will appreciate if someone can guide me on the exact process/ method for programming the Micro.
Thanks in advance