Part Number: MSP430FR5969
Hi,
I'm trying to place some persistent variables into FRAM on the MSP430FR5969 using the current GCC compiler. I am using a make file to build the project. I do NOT use CCS ide. I have checked that the linker script has a .PERSISTENT section declared, but am unable to get the variable to change. For example:
void myFunction(void)
{
__attribute__ ((persistent)) uint8_t count = 0;
printf("The count:%u", count++);
}
when I call myFunction(), count does not increment. Everything compiles ok, and there is a .persistent. segment reported by the linker.
Any ideas as to why I can't get count to increment?
Thanks,
Peter Philippa.