This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

fr5994 real FFT result

i am  using FR5994 to analysis signal ,the signal is made of two signals:

1、singal with frequency 200Hz,amplitude  0.6

2、signal with frequency 2100Hz,amplitude 0.15

the Fs = 8192Hz,after N = 256 point real FFT ,the result coming into being as the figure above.

so  what's the figure above representation? for example, what is [13,7305]  mean?

that is to say how can i get the Frequency-Amplitude  of  the signal from the figure?

  • Kissn Liu said:
    so  what's the figure above representation?

    Based on the information presented not sure.

    How was the figure produced?

  • #include "msp430.h"

    #include <math.h>
    #include <stdint.h>
    #include <stdbool.h>

    #include "DSPLib.h"

    /* Input signal parameters */
    #define FS 8192
    #define SAMPLES 256
    #define SIGNAL_FREQUENCY1 200
    #define SIGNAL_AMPLITUDE1 0.6
    #define SIGNAL_FREQUENCY2 2100
    #define SIGNAL_AMPLITUDE2 0.15

    /* Hamming window parameters */
    #define HAMMING_ALPHA 0.53836
    #define HAMMING_BETA 0.46164

    /* Constants */
    #define PI 3.1415926536

    /* Generated Hamming window function */
    DSPLIB_DATA(window,4)
    _q15 window[SAMPLES];

    /* Input signal and FFT result */
    DSPLIB_DATA(input,MSP_ALIGN_FFT_Q15(SAMPLES))
    _q15 input[SAMPLES];

    /* Temporary data array for processing */
    DSPLIB_DATA(temp,4)
    _q15 temp[3*SAMPLES/2];

    /* Benchmark cycle counts */
    volatile uint32_t cycleCount;

    /* Function prototypes */
    extern void initSignal(void);
    extern void initHamming(void);

    void main(void)
    {
    msp_status status;
    msp_mpy_q15_params mpyParams;
    msp_fft_q15_params fftParams;

    /* Disable WDT */
    WDTCTL = WDTPW + WDTHOLD;

    /* Initialize input signal and Hamming window */
    initSignal();
    initHamming();

    /* Multiply input signal by generated Hamming window */
    mpyParams.length = SAMPLES;
    status = msp_mpy_q15(&mpyParams, input, window, input);
    msp_checkStatus(status);

    /* Initialize the fft parameter structure. */
    fftParams.length = SAMPLES;
    fftParams.bitReverse = true;
    fftParams.twiddleTable = msp_cmplx_twiddle_table_256_q15;

    /* Perform real FFT with fixed scaling */
    msp_benchmarkStart(MSP_BENCHMARK_BASE, 16);
    status = msp_fft_fixed_q15(&fftParams, input);
    cycleCount = msp_benchmarkStop(MSP_BENCHMARK_BASE);
    msp_checkStatus(status);

    /* End of program. */
    __no_operation();
    }

    void initSignal(void)
    {
    msp_status status;
    msp_add_q15_params addParams;
    msp_sinusoid_q15_params sinParams;

    /* Generate Q15 input signal 1 */
    sinParams.length = SAMPLES;
    sinParams.amplitude = _Q15(SIGNAL_AMPLITUDE1);
    sinParams.cosOmega = _Q15(cosf(2*PI*SIGNAL_FREQUENCY1/FS));
    sinParams.sinOmega = _Q15(sinf(2*PI*SIGNAL_FREQUENCY1/FS));
    status = msp_sinusoid_q15(&sinParams, input);
    msp_checkStatus(status);

    /* Generate Q15 input signal 2 to temporary array */
    sinParams.length = SAMPLES;
    sinParams.amplitude = _Q15(SIGNAL_AMPLITUDE2);
    sinParams.cosOmega = _Q15(cosf(2*PI*SIGNAL_FREQUENCY2/FS));
    sinParams.sinOmega = _Q15(sinf(2*PI*SIGNAL_FREQUENCY2/FS));
    status = msp_sinusoid_q15(&sinParams, temp);
    msp_checkStatus(status);

    /* Add input signals */
    addParams.length = SAMPLES;
    status = msp_add_q15(&addParams, input, temp, input);
    msp_checkStatus(status);
    }

    void initHamming(void)
    {
    msp_status status;
    msp_sub_q15_params subParams;
    msp_copy_q15_params copyParams;
    msp_fill_q15_params fillParams;
    msp_sinusoid_q15_params sinParams;

    /* Generate sinusoid for cosine function */
    sinParams.length = 3*SAMPLES/2;
    sinParams.amplitude = _Q15(HAMMING_BETA);
    sinParams.cosOmega = _Q15(cosf(2*PI/(SAMPLES-1)));
    sinParams.sinOmega = _Q15(sinf(2*PI/(SAMPLES-1)));
    status = msp_sinusoid_q15(&sinParams, temp);
    msp_checkStatus(status);

    /* Shift sinusoid by pi/2 to create cosine function */
    copyParams.length = SAMPLES;
    status = msp_copy_q15(&copyParams, &temp[SAMPLES/4], &temp[0]);
    msp_checkStatus(status);

    /* Fill temporary array with alpha constant */
    fillParams.length = SAMPLES;
    fillParams.value = _Q15(HAMMING_ALPHA);
    status = msp_fill_q15(&fillParams, window);
    msp_checkStatus(status);

    /* Subtract generated cosine from alpha constant to generate final window */
    subParams.length = SAMPLES;
    status = msp_sub_q15(&subParams, window, temp, window);
    msp_checkStatus(status);
    }

    after doing FFT,the result about the figure is the array of which the input pointer point to.

    status = msp_fft_fixed_q15(&fftParams, input);

  • Kissn Liu said:
    after doing FFT,the result about the figure is the array of which the input pointer point to.

    The posted code appears to be the MSP DSP Library transform_ex1_fft_fixed_q15.c example.

    Does the following description of the example help answer your question?

    This example demonstrates how to use the msp_fft_fixed_q15 API to transform a real input data array to the frequency domain using the Q15 fast fourier transform (FFT) with fixed scaling. The real FFT function is identical to running a complex FFT with imaginary components set to zero. The result of the real FFT is a complex vector with half the samples but identical byte length.

    See Computing a Length N/2 Complex FFT from a Length N Real Input Sequence for some more information.

  • OK I know what the out put of the FFT fuction measn. by the way, does the LEA support higher point FFT?
    for example 512 ,1024.....
  • Kissn Liu said:
    by the way, does the LEA support higher point FFT?

    From looking at the MSP DSP Library documentation LEA supports FFTs of size 16, 32, 64, 128, 256, 512, 1024, 2048 or 4096.

    Those are the FFT sizes for which Twiddle factor tables are stored in the LEA ROM (or the DSPLib source code for the non LEA versions).

**Attention** This is a public forum