Hi,
i just recently got a development board with this chip. Still finding my way trough the MSP430 ecosystem, so i apologize for the ignorance.
I was wondering what options do i have to reduce power consumptions in active mode?
Thing is, a custom board will eventually run on a solar panel, with no battery. That means i'll have unlimited capacity, but limited power.
The "energy trace" tool shows current consumption around 0,4mA, @3MHz. I switched to the VLOCLK at 10kHz, an it reads at 0,2mA, which sounds much to high in comparison. I'm guessing i must be doing something wrong.
Any pointers or suggestions?
Thanks