Other Parts Discussed in Thread: MSP-EXP430FR2311, MSP-EXP430FR2433, MSP-EXP430FR4133
Hello,
This is my very first post to this forum so sorry in advance for any kind of noob usage experience :)
I 've been playing with MSP EXP430G2 Rev 1.5 Launchpad for a while but I have detected an issue with the Application UART on Windows 10 (I don't want to mean issue is caused by Windows 10 driver, I wanted to emphasize the OS I am using).
The issue is, Application UART is very unstable. This I mean, I need to unplug/replug several times before I can successfully get a character sent from my laptop via Termite terminal (I've tried TerraTerm and RealTerm also, result is the same).
I am very sure that the issue is not caused by the MSP430G2553 device installed on the launchpad because I tried a loopback connection bypassing the G2553 and result is the same.
Also, I tried using a FTDI USB to Serial Adapter by disconnecting the G2553's Tx/Rx pins from Application UART and connecting them to the FTDI adapter and voila, all success, G2553 can get what I send from PC flawlessly.
I really like to play this Launchpad and the device, I would like some kind of firmware update for the Emulation part of the Launchpad or a possible Windows driver update. Any specific questions, please ask and I will answer for you to further analyze the issue.
Thanks in advance!