Part Number: MSP430FR6047
Hi,
I have a simple question. Is there a simple formula to link amplitude from ADC capture to the input signal of the ADC?
I'm trying to link the amplitude of the input signal of ADC (observed on scope) with the values given in the USS Design Center (observed on ADC capture TAB).
Below is what I measure, with gain control=21.5 dB (means amplification is 11.88):
Approximatively we have 1800 peak-to-peak amplitude on ADC capture and 50mVpp on scope.
I would expect to get 50mV * 11.88 = 594mVpp on ADC capture. If the amplitude unit is in mV...
Obviously I miss something...
Also, what is the unit of the amplitude scale?
Appreciate your help.
Best Regards,
Thierry Soubie