Part Number: MSP430FR5969
Other Parts Discussed in Thread: MSPBSL
Tool/software: Code Composer Studio
Hi there,
I'm developing an application with MSP430FR5969, usind Code Composer Studio 7.4.
I need to provide an utility for "On field software update". I'm trying to understand if I can perform a software update without BSL utilities.
Is there a way I can update the software with the .hex file generated by the compiler runtime? I'm planning to create a CUSTOM uart communication that would let a terminal (Teraterm) send the .hex file and directly copy it to the onchip memory and create a custom code that will perform the software update so that it will be executed at startup: how can I do it? Are there examples as a reference?
Thank you
Regards