Part Number: MSP430FR5969
I want to use Port J pin 6 and 7 as Output on MSP430Fr5969 Controller.
During GPIO initialization , all the ports are made output and low using following instructions:
P1DIR = 0xFF;
P2DIR = 0xFF;
P3DIR = 0xFF;
P4DIR = 0xFF;
PJDIR = 0xFFFF;
P1OUT =0x00;
P2OUT =0x00;
P3OUT =0x00;
P4OUT =0x00;
PJOUT =0x0000;
But when I try to put GPIO 6 and 7 of Port J high, it does not set the pin high..
Is there any special settings for Port J on MSP430Fr5969 controller since pins on Port J are shared with JTAG connection as well.
I am using GPIO_setOutputHighOnPin(GPIO_PORT_PJ,GPIO_PIN6) to set the pin High
Same thing is also observed with Port 1 Pin 6 and pin 7.
Let me know if I have missed something
With Regards
Aalakh Devari