Part Number: MSP430FR5969
Hi,
My customer who is evaluating MSP430FR5969 has a question for GPIO pad impedance.
According to Datasheet table 5-11, High-impedance input leakage current is +/-20nA.
But if customer measured it on their custom board, the leakage seems much higher.
For example, if customer put an external pull up(3.0V) with 1M Ohm on P4.7 or P1.3, the voltage drops to ~2.7V.
Please note that the pin is open(nothing other than pull-up and 0.1uF capacitor are connected).
If an external pull-up value is changed to 100kOhm, the voltage is ~3V.
What is causing such behavior?
Thanks and regards,
Koichiro Tashiro