Part Number: MSP430FR6047
Other Parts Discussed in Thread: MSP430FR6989
Hi Team,
This is customer request, can you please advise:
"
1. I use the USS library 02_20_00_18 version for MSP430FR6047. In our flowmeters, we found that the delta TOF values calculated by the USS sometimes deteriorated interestingly, and as a result of these incorrect TOF values, the device made incorrect calculations in the water velocity and thus flow calculations.
2. Again, a different problem we have with MSP430FR6047; UART communication with MCU crashes after BSL mass erasing and I cannot communicate any more. (which I never had such a problem with MSP430FR6989. Both MCUs have the same BSL structure)
3. This will be of the nature of advice;
We use DN60, DN80 and DN100 pipe diameters in our systems. 1MHZ ultrasonic sensors are angled 45 degrees facing each other. In the field, the devices are generally operated at a pressure of 2-3 bar with nominal 30-50 m3 / h flow rate and land water. Is MSP430FR6047 suitable for this build? Because in the examples on the internet, the sensors are used in a U-shaped layout and small diameter pipes. What are your recommendations for a precise measurement?
"
Thanks in advance
Best Regards
Furkan Sefiloglu