Other Parts Discussed in Thread: MSP430F2274
I am planning on using the Epson MC-146 32.768kHz crystal with a msp430F2274. The load capacitance of the crystal is 9 pF. I am unclear in the documentation what value I should set for xCAP. I can choose between 1, 6, 10, and 12.5 pF. Should this value match the load capacitance of the crystal or does it represent the individual values for each capacitor, CL1 and CL2? What value should I choose?
Thanks.