As the title suggests, I'm working to port this example so I'll have a guide to go by when operating with the MPU-6050. The INT pin on the MPU-6050 is configured to generate an interrupt for the Tiva C Launchpad (running at 80MHz). The problem is that the pin never changes to indicate data is ready and thus never generates an interrupt on the Tiva C. Here's a snippet of the altered example and almost everything else about the example has been kept the same (except for renaming functions and variables to MPU6050 instead of MPU9150 and including the appropriate headers):
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
ConfigureUART();
UARTprintf("\033[2JMPU6050 Raw Example\n");
g_pui32Colors[RED] = 0x8000;
g_pui32Colors[BLUE] = 0x8000;
g_pui32Colors[GREEN] = 0x0000;
RGBInit(0);
RGBColorSet(g_pui32Colors);
RGBIntensitySet(0.5f);
RGBEnable();
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C3);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
ROM_GPIOPinConfigure(GPIO_PD0_I2C3SCL);
ROM_GPIOPinConfigure(GPIO_PD1_I2C3SDA);
GPIOPinTypeI2CSCL(GPIO_PORTD_BASE, GPIO_PIN_0);
ROM_GPIOPinTypeI2C(GPIO_PORTD_BASE, GPIO_PIN_1);
ROM_GPIOPinTypeGPIOInput(GPIO_PORTE_BASE, GPIO_PIN_2);
GPIOIntEnable(GPIO_PORTE_BASE, GPIO_PIN_2);
ROM_GPIOIntTypeSet(GPIO_PORTE_BASE, GPIO_PIN_2, GPIO_FALLING_EDGE);
ROM_IntEnable(INT_GPIOE);
ROM_IntMasterEnable();
ROM_SysCtlPeripheralClockGating(true);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_TIMER0);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_TIMER1);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_I2C3);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_WTIMER5);
I2CMInit(&g_sI2CInst, I2C3_BASE, INT_I2C3, 0xff, 0xff,
ROM_SysCtlClockGet());
MPU6050Init(&g_sMPU6050Inst, &g_sI2CInst, MPU6050_I2C_ADDRESS,
MPU6050AppCallback, &g_sMPU6050Inst);
MPU6050AppI2CWait(__FILE__, __LINE__);
// Start here
g_sMPU6050Inst.pui8Data[0] = MPU6050_CONFIG_DLPF_CFG_94_98;
g_sMPU6050Inst.pui8Data[1] = MPU6050_GYRO_CONFIG_FS_SEL_250;
g_sMPU6050Inst.pui8Data[2] = (MPU6050_ACCEL_CONFIG_AFS_SEL_2G);
MPU6050Write(&g_sMPU6050Inst, MPU6050_O_CONFIG, g_sMPU6050Inst.pui8Data, 3,
MPU6050AppCallback, &g_sMPU6050Inst);
MPU6050AppI2CWait(__FILE__, __LINE__);
g_sMPU6050Inst.pui8Data[0] = MPU6050_INT_PIN_CFG_INT_LEVEL |
MPU6050_INT_PIN_CFG_INT_RD_CLEAR |
MPU6050_INT_PIN_CFG_LATCH_INT_EN;
g_sMPU6050Inst.pui8Data[1] = MPU6050_INT_ENABLE_DATA_RDY_EN;
MPU6050Write(&g_sMPU6050Inst, MPU6050_O_INT_PIN_CFG,
g_sMPU6050Inst.pui8Data, 2, MPU6050AppCallback,
&g_sMPU6050Inst);
MPU6050AppI2CWait(__FILE__, __LINE__);
CompDCMInit(&g_sCompDCMInst, 1.0f / 50.0f, 0.2f, 0.8f, 0.0f);
UARTprintf("\033[2J\033[H");
UARTprintf("MPU6050 6-Axis Simple Data Application Example\n\n");
UARTprintf("\033[20GX\033[31G|\033[43GY\033[54G|\033[66GZ\n\n");
UARTprintf("Accel\033[8G|\033[31G|\033[54G|\n\n");
UARTprintf("Gyro\033[8G|\033[31G|\033[54G|\n\n");
UARTprintf("Mag\033[8G|\033[31G|\033[54G|\n\n");
UARTprintf("\n\033[20GRoll\033[31G|\033[43GPitch\033[54G|\033[66GYaw\n\n");
UARTprintf("Eulers\033[8G|\033[31G|\033[54G|\n\n");
UARTprintf("\n\033[17GQ1\033[26G|\033[35GQ2\033[44G|\033[53GQ3\033[62G|"
"\033[71GQ4\n\n");
UARTprintf("Q\033[8G|\033[26G|\033[44G|\033[62G|\n\n");
RGBBlinkRateSet(1.0f);
ui32CompDCMStarted = 0;
while(1){
//
// Go to sleep mode while waiting for data ready.
//
while(!g_vui8I2CDoneFlag)
{
ROM_SysCtlSleep();
}
//
// Clear the flag
//
g_vui8I2CDoneFlag = 0; // This point is never reached.
I2C3 is setup on port pins PD0 and PD1 to communicate with the MPU-6050 while the interrupt pin is set to PE2. Something that I noticed in the debugger is that after the interrupt logic level MPU6050_INT_PIN_CFG_INT_LEVEL write is performed the Port E Data register indicates that a change from 0 to 1 does occur on PE2 (which is correct operation but beyond that it never goes low no matter what even if a read on the MPU6050 is performed). If anyone has any suggestions for what wrong thing I am doing, feel free to chime in. I'm using CCS version 5.5 and am using TivaWare version 2.0.1.11577
EDIT: Upon further investigation, the MPU6050DataRead function is always returning true but the values are never updated for use by the MPU6050DataAccelGetFloat and MPU6050DataGyroGetFloat. Both of those functions are always storing zeroes for some reason.