First time posting in TI forums!
I've had a Tiva C Launchpad for quite some time now (about 1.5 years), and I just noticed that the red LED is not lighting up anymore. At first, I thought I was not configuring the pin properly, but then applied the same configuration to PF1, PF2 and PF3. Blue and Green LEDs are working fine.
I can write to the to the register just fine, and tried a red LED with a 470 ohm resistor on a breadboard attached to PF1 and it's working fine.
To me, it seems the red LED is busted, but since I'm a newbie in electronics, I would appreciate some validation. Is there any other reason to this problem?
Also, how hard would it be to replace D1? It looks like I would need a special iron tip, and my soldering skills are not very good.
Thanks for your help!