Hi. I've been chasing a problem for hours. DHCP works fine but the static IP is screwed up (and I need both to work).
I'm even using the latest and greatest tivaware 2.1.4.178.
I do have #define LWIP_DHCP 1 because the customer will be able to use DHCP or assign a static ip.
I finally traced what appears to be the problem to a little function called lwIPLinkDetect();
It wipes out the IP address (this is in lwiplib.c):
// // Clear any address information from the network interface. // ip_addr.addr = 0; net_mask.addr = 0; gw_addr.addr = 0; netif_set_addr(&g_sNetIF, &ip_addr, &net_mask, &gw_addr);
I added this right above as a fix: if (g_ui32IPMode == IPADDR_USE_STATIC) return;
I'm not sure if I was just doing something wrong or what was going on but for anybody that has the same problem I'm posting the complete function below with the fix in it.
//***************************************************************************** // // This function performs a periodic check of the link status and responds // appropriately if it has changed. // //***************************************************************************** #if LWIP_AUTOIP || LWIP_DHCP static void lwIPLinkDetect(void) { bool bHaveLink; struct ip_addr ip_addr; struct ip_addr net_mask; struct ip_addr gw_addr; // // See if there is an active link. // bHaveLink = MAP_EMACPHYRead(EMAC0_BASE, PHY_PHYS_ADDR, EPHY_BMSR) & EPHY_BMSR_LINKSTAT; // // Return without doing anything else if the link state hasn't changed. // if(bHaveLink == g_bLinkActive) { return; } // // Save the new link state. // g_bLinkActive = bHaveLink; if (g_ui32IPMode == IPADDR_USE_STATIC) return; // // Clear any address information from the network interface. // ip_addr.addr = 0; net_mask.addr = 0; gw_addr.addr = 0; netif_set_addr(&g_sNetIF, &ip_addr, &net_mask, &gw_addr); // // See if there is a link now. // if(bHaveLink) { // // Start DHCP, if enabled. // #if LWIP_DHCP if(g_ui32IPMode == IPADDR_USE_DHCP) { dhcp_start(&g_sNetIF); } #endif // // Start AutoIP, if enabled and DHCP is not. // #if LWIP_AUTOIP if(g_ui32IPMode == IPADDR_USE_AUTOIP) { autoip_start(&g_sNetIF); } #endif } else { // // Stop DHCP, if enabled. // #if LWIP_DHCP if(g_ui32IPMode == IPADDR_USE_DHCP) { dhcp_stop(&g_sNetIF); } #endif // // Stop AutoIP, if enabled and DHCP is not. // #if LWIP_AUTOIP if(g_ui32IPMode == IPADDR_USE_AUTOIP) { autoip_stop(&g_sNetIF); } #endif } } #endif