Part Number: EK-TM4C1294XL
Tool/software: TI-RTOS
Hello;
In TI-RTOS concept hardware interrupt in workshop series , the first lab about usage of hardware interrup by blinking a led.While I am trying this lab I faced with some problem. In code , the hwi will occur based on Tiva TM4c1294xl Timer 2A.But when I set the properties of hwi with dynamically nothing happens.The all code is below;
#include <xdc/std.h>
#include <xdc/runtime/System.h>
/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/hal/Timer.h>
/* TI-RTOS Header files */
// #include <ti/drivers/EMAC.h>
#include <ti/drivers/GPIO.h>
// #include <ti/drivers/I2C.h>
// #include <ti/drivers/SDSPI.h>
// #include <ti/drivers/SPI.h>
// #include <ti/drivers/UART.h>
// #include <ti/drivers/USBMSCHFatFs.h>
// #include <ti/drivers/Watchdog.h>
// #include <ti/drivers/WiFi.h>
/* Board Header file */
#include "Board.h"
#define TASKSTACKSIZE 512
Hwi_Handle hwi1;
Void hwiFxn(){
GPIO_write(Board_LED1,Board_LED_ON);
}
int main(void)
{
Hwi_Params hwiP;
Task_Params taskParams;
/* Call board init functions */
Board_initGeneral();
// Board_initEMAC();
Board_initGPIO();
// Board_initI2C();
// Board_initSDSPI();
// Board_initSPI();
// Board_initUART();
// Board_initUSB(Board_USBDEVICE);
// Board_initUSBMSCHFatFs();
// Board_initWatchdog();
// Board_initWiFi();
/* Construct heartBeat Task thread */
Task_Params_init(&taskParams);
taskParams.arg0 = 1000;
taskParams.stackSize = TASKSTACKSIZE;
taskParams.stack = &task0Stack;
Task_construct(&task0Struct, (Task_FuncPtr)heartBeatFxn, &taskParams, NULL);
Hwi_Params_init(&hwiP);
hwiP.arg=0;
hwiP.eventId=39;
hwiP.priority=0;
hwi1=Hwi_create(39,hwiFxn,&hwiP,NULL);
/* Turn on user LED */
GPIO_write(Board_LED0, Board_LED_ON);
GPIO_write(Board_LED1, Board_LED_OFF);
System_printf("Starting the example\nSystem provider is set to SysMin. "
"Halt the target to view any SysMin contents in ROV.\n");
/* SysMin will only print to the console when you call flush or exit */
System_flush();
/* Start BIOS */
BIOS_start();
return (0);
}
Also, in the workshop it says about Event id like for Tiva C Series;
I wonder that I am missing some point while setting Hardware Interrup? It would be very helpful to understand usage and settings for further use.
Best Regards,