Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Hello ,
I write this conditional ssi algorithm for my projects but there is an error while i am debugging. I debug this code step by step and ssidataget() function ( in data_receive() ) is error. What can i for stop this ??
#include <stdio.h>
#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include <math.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_can.h"
#include "inc/hw_ints.h"
#include "inc/hw_gpio.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/gpio.h"
#include "driverlib/uart.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/pwm.h"
#include "driverlib/rom.h"
#include "driverlib/i2c.h"
#include "driverlib/rom_map.h"
#include "driverlib/watchdog.h"
#include "driverlib/adc.h"
#include "driverlib/can.h"
#include "driverlib/eeprom.h"
#include "driverlib/timer.h"
#include "driverlib/ssi.h"
bool isAdcReadOk;
#define NUM_SSI_DATA 3
uint32_t ui32ADC0Value[3];
uint32_t ui32Index;
uint32_t ulindex;;
uint32_t Data_Alinan[3];
#define PIN_LOW 0x00
#define PIN_HIGH 0xFF
void adckesme(void)
{
ADCIntClear(ADC0_BASE, 3);
ADCSequenceDataGet(ADC0_BASE , 3, ui32ADC0Value);
}
void SSI_DATA_BAS(uint32_t SSI_NUMBER,uint32_t *DATA)
{
for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
{
SSIDataPut(SSI_NUMBER, *DATA); //// requesting data
}
}
void data_receive(void)
{
// GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, PIN_LOW);
for(ui32Index=0 ; ui32Index < 3 ; ui32Index++){
SSIDataGet(SSI0_BASE, &Data_Alinan[0]);
}
Data_Alinan[0] &= 0x00FF;
Data_Alinan[1] &= 0x00FF;
Data_Alinan[2] &= 0x00FF;
while(SSIBusy(SSI0_BASE)){};
// GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, PIN_HIGH);
}
void InitConsole_SPI(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA2_SSI0CLK);
// GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinConfigure(GPIO_PA4_SSI0RX);
GPIOPinConfigure(GPIO_PA5_SSI0TX);
GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 |GPIO_PIN_2);
SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,SSI_MODE_SLAVE, 2000000, 8);
SSIEnable(SSI0_BASE);
}
int main(void)
{
SysCtlClockSet(SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ|SYSCTL_SYSDIV_5);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
ADCHardwareOversampleConfigure(ADC0_BASE,64);
ADCSequenceDisable(ADC0_BASE, 3);
ADCSequenceConfigure(ADC0_BASE , 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 3, 0 , ADC_CTL_TS|ADC_CTL_IE|ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, 3);
ADCIntEnable(ADC0_BASE, 3);
ADCIntRegister(ADC0_BASE, 3, adckesme);
IntEnable(INT_ADC0SS3);
InitConsole_SPI();
while(1)
{
ADCProcessorTrigger(ADC0_BASE , 3);
// while(SSIBusy(SSI0_BASE)){};
data_receive();
// while(SSIBusy(SSI0_BASE)){};
if(Data_Alinan[0]==1){ ///// Did the data request come ?
if(ui32ADC0Value[0] != 0 ){ //// Is there data in adc ?
SSI_DATA_BAS(SSI0_BASE , ui32ADC0Value);
}
}
}
}