Other Parts Discussed in Thread: TMP006
Hi,
I'm triying get data from TMP006EVM via I2C, with eclipse, when reading values from the booster, always get the same result. I think the I2C reading code is wrong, but i'm not sure.
The code is adapted from: https://github.com/adafruit/Adafruit_TMP006
(The relevant parts are in TMP6_Read16 and TMP6_Write16)
Here is the code:
/**
** TMP006 EVM + UART
**
**/
#include <stdint.h>
#include <stdbool.h>
#include <inc/tm4c123gh6pge.h>
//#include <utils/ustdlib.h>
#include <inc/hw_memmap.h>
#include <inc/hw_types.h>
#include <inc/hw_nvic.h>
#include <driverlib/systick.h>
#include <driverlib/gpio.h>
#include <driverlib/pin_map.h>
#include <driverlib/sysctl.h>
#include <driverlib/debug.h>
#include <driverlib/i2c.h>
#include <driverlib/uart.h>
#include <driverlib/timer.h>
#include <utils/uartstdio.h>
#define SYSTICK_INT_PRIORITY 0x80
#include <inc/hw_ints.h>
#include <driverlib/interrupt.h>
#include "UART_TMP006.h"
void UARTIntHandler(void);
//#if POLLING == 0
void UARTIntHandler(void){}
// uint32_t ui32Status;
// // GET INSTERRUPT STATUS
// ui32Status = UARTIntStatus(UART0_BASE, true);
// // CLEAR ASSERTED INTERRUPTS
// UARTIntClear(UART0_BASE, ui32Status);
//
// // LOOP WHILE THERE ARE CHARS
// while(UARTCharsAvail(UART0_BASE)){
// // ECHO CHARACTER
// UARTCharPutNonBlocking(UART0_BASE, UARTCharGetNonBlocking(UART0_BASE));
// // BLINK LED
// GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1);
// // DELAY ~1ms
// SysCtlDelay(SysCtlClockGet() / (1000 * 3));
// // TURN OFF LED
// GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x00);
// }
//}
//#endif
int main(void);
void InitUART(void);
void InitI2C(void);
void InitLeds(void);
void InitBoardLeds(void);
void InitSysTick(void);
void InitTimer(void);
void BoardLeds(uint8_t);
void SysTickWait(uint32_t);
void SysTickWait_ms(uint32_t);
uint8_t TMP6_Start(void);
uint16_t TMP6_Read16(uint8_t);
void TMP6_Write16(uint8_t, uint16_t);
void InitUART(void){
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
}
void InitI2C(void){
// INITIALIZE I2C PERIPH 3
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C3);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
I2CMasterInitExpClk(I2C3_BASE, SysCtlClockGet(), false);
GPIOPinConfigure(GPIO_PD1_I2C3SDA);
GPIOPinConfigure(GPIO_PD0_I2C3SCL);
GPIOPinTypeI2C(GPIO_PORTD_BASE, GPIO_PIN_1);
GPIOPinTypeI2CSCL(GPIO_PORTD_BASE, GPIO_PIN_0);
}
void InitLeds(void){
// ENABLE LEDS
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1); // LED PF1
}
void InitBoardLeds(void){
// ENABLE BOARD LEDS
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_3 | GPIO_PIN_2);
}
void InitSysTick(void){
// DEFAULTS TO 1ms
//uint32_t microsecs = F_CPU / SYSTICK_MHZ;
//SysTickPeriodSet(microsecs * 1000);
// 40000 > 0.001s > 1ms
SysTickPeriodSet(40000);
SysTickEnable();
IntPrioritySet(FAULT_SYSTICK, SYSTICK_INT_PRIORITY);
SysTickIntEnable();
}
void InitTimer(void){
uint32_t ui32Period;
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
ui32Period = (SysCtlClockGet() / 2) / 2;
TimerLoadSet(TIMER0_BASE, TIMER_A, ui32Period - 1);
IntEnable(INT_TIMER0A);
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
IntMasterEnable();
TimerEnable(TIMER0_BASE, TIMER_A);
}
void SysTickWait(uint32_t delay){
// 0x00FFFFFF > 16777215 > 0.42s(40MHZ)
// 120MHz > nS
// 80MHz > 12.5nS
// 40MHz > 25.nS
// 16MHz > 62.5nS
// FORCE RELOAD
HWREG(NVIC_ST_CURRENT) = 0;
// ENABLE SysTick
SysTickEnable();
uint32_t test = SysTickValueGet();
for(uint32_t aux = 0; aux < delay; aux++) {
while (test > 0){
test = SysTickValueGet();
__asm__("NOP");
}
}
}
void SysTickWait_ms(uint32_t delay){
if (delay == 0) {
SysTickWait(1);
}
SysTickWait(delay);
}
void BoardLeds(uint8_t onoff){
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, 0x8);
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_2, 0x4);
}
int main(void){
// 400MHz > DEFAULT /2 > /5 > 40MHz
// 40MHz SYSTEM CLOCK
SysCtlClockSet(SYSCTL_SYSDIV_5 |SYSCTL_USE_PLL |
SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);
InitUART();
InitI2C();
InitLeds();
InitBoardLeds();
InitSysTick();
//InitTimer();
UARTStdioConfig(0, 115200, 40000000);
// // CONFIG UART
// UARTConfigSetExpClk(UART0_BASE, SysCtlClockGet(), 115200,
// UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE);
//
// // ENABLE INTERRUPTS
// IntMasterEnable();
// // ENABLE UART INTERRUPTS
// IntEnable(INT_UART0);
// // ENABLE RX AND TX INTERRUPTS
// UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);
//
UARTprintf("Hello world!\n");
UARTprintf("\n");
UARTprintf("%u", SysCtlClockGet());
UARTprintf("\n");
BoardLeds(0);
uint8_t val;
val = TMP6_Start();
UARTprintf("TMP_START: "); UARTprintf("%u", val); UARTprintf("\n");
while(true){}
}
uint8_t TMP6_Start(void){
TMP6_Write16(TMP006_CONFIG, TMP006_CFG_MODEON | TMP006_CFG_DRDYEN | TMP006_CFG_16SAMPLE);
uint16_t mid, did;
mid = TMP6_Read16(TMP006_MANID);
did = TMP6_Read16(TMP006_DEVID);
#ifdef TMP006_DEBUG
UARTprintf("mid = 0x"); UARTprintf("%X", mid); UARTprintf("\n");
UARTprintf("did = 0x"); UARTprintf("%X", did); UARTprintf("\n");
#endif
if (mid != 0x5449) return 0;
if (did != 0x67) return 0;
return 1;
}
uint16_t TMP6_Read16(uint8_t u8Addr) {
uint16_t u16Return;
uint32_t u32Aux;
// SENDS REGISTER ADDRESS TO READ FROM
I2CMasterSlaveAddrSet(I2C3_BASE, TMP006_I2C_ADDR, true);
I2CMasterDataPut(I2C3_BASE, u8Addr);
I2CMasterControl(I2C3_BASE, I2C_MASTER_CMD_SINGLE_SEND);
while(I2CMasterBusy(I2C3_BASE)){}
I2CMasterSlaveAddrSet(I2C3_BASE, TMP006_I2C_ADDR, true);
I2CMasterControl(I2C3_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
while(I2CMasterBusy(I2C3_BASE)){}
u32Aux = I2CMasterDataGet(I2C3_BASE);
u16Return = ((u32Aux<<8) | 0x0000FF00);
//I2CMasterSlaveAddrSet(I2C3_BASE, TMP006_I2C_ADDR, true);
I2CMasterControl(I2C3_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
while(I2CMasterBusy(I2C3_BASE)){}
u32Aux = I2CMasterDataGet(I2C3_BASE);
u16Return |= u32Aux;
return u16Return;
}
void TMP6_Write16(uint8_t u8Addr, uint16_t u16Data){
// SENDS REGISTER ADDRESS TO READ FROM
I2CMasterSlaveAddrSet(I2C3_BASE, TMP006_I2C_ADDR, true);
I2CMasterDataPut(I2C3_BASE, u8Addr);
I2CMasterControl(I2C3_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusy(I2C3_BASE)){}
//
//I2CMasterSlaveAddrSet(I2C3_BASE, TMP006_I2C_ADDR, true);
I2CMasterControl(I2C3_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
I2CMasterDataPut(I2C3_BASE, u16Data >> 8);
while(I2CMasterBusy(I2C3_BASE)){}
//I2CMasterControl(I2C3_BASE, I2C_MASTER_CMD_SINGLE_SEND);
//while(I2CMasterBusy(I2C3_BASE)){}
//
//I2CMasterSlaveAddrSet(I2C3_BASE, TMP006_I2C_ADDR, true);
I2CMasterControl(I2C3_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
I2CMasterDataPut(I2C3_BASE, u16Data);
while(I2CMasterBusy(I2C3_BASE)){}
//I2CMasterControl(I2C3_BASE, I2C_MASTER_CMD_SINGLE_SEND);
//while(I2CMasterBusy(I2C3_BASE)){}
}
// SYSTICK ISR
void SysTickIntHanhdler(void) {
// if (GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_1)){
// GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PORTF_BASE & 0xfd); //SOLO LIMPIAR BIT 3 1000
// } else {
// GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x02);
// }
}
// TIMER0 ISR
void Timer0IntHandle(void){
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
if (GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_1)){
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PORTF_BASE & 0xfd);
} else {
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x02);
}
}
Best regards