I noticed that the TivaWare_C_Series-2.2.0.295/examples/peripherals/epi/sdram.c contains a block of DRM code to set the EPI pin-muxing:
// // This step configures the internal pin muxes to set the EPI pins for use // with EPI. Please refer to the datasheet for more information about pin // muxing. Note that EPI0S27:20 are not used for the EPI SDRAM // implementation. // TODO: Update this section based upon the EPI pin assignment on your // target part. // // // EPI0S4 ~ EPI0S7: C4 ~ 7 // ui32Val = HWREG(GPIO_PORTC_BASE + GPIO_O_PCTL); ui32Val &= 0x0000FFFF; ui32Val |= 0xFFFF0000; HWREG(GPIO_PORTC_BASE + GPIO_O_PCTL) = ui32Val; // // EPI0S8 ~ EPI0S9: A6 ~ 7 // ui32Val = HWREG(GPIO_PORTA_BASE + GPIO_O_PCTL); ui32Val &= 0x00FFFFFF; ui32Val |= 0xFF000000; HWREG(GPIO_PORTA_BASE + GPIO_O_PCTL) = ui32Val; // // EPI0S10 ~ EPI0S11: G0 ~ 1 // ui32Val = HWREG(GPIO_PORTG_BASE + GPIO_O_PCTL); ui32Val &= 0xFFFFFF00; ui32Val |= 0x000000FF; HWREG(GPIO_PORTG_BASE + GPIO_O_PCTL) = ui32Val; // // EPI0S12 ~ EPI0S15: M0 ~ 3 // ui32Val = HWREG(GPIO_PORTM_BASE + GPIO_O_PCTL); ui32Val &= 0xFFFF0000; ui32Val |= 0x0000FFFF; HWREG(GPIO_PORTM_BASE + GPIO_O_PCTL) = ui32Val; // // EPI0S16 ~ EPI0S19: L0 ~ 3 // ui32Val = HWREG(GPIO_PORTL_BASE + GPIO_O_PCTL); ui32Val &= 0xFFFF0000; ui32Val |= 0x0000FFFF; HWREG(GPIO_PORTL_BASE + GPIO_O_PCTL) = ui32Val; // // EPI0S28 : B3 // ui32Val = HWREG(GPIO_PORTB_BASE + GPIO_O_PCTL); ui32Val &= 0xFFFF0FFF; ui32Val |= 0x0000F000; HWREG(GPIO_PORTB_BASE + GPIO_O_PCTL) = ui32Val; // // EPI0S29 ~ EPI0S30: N2 ~ 3 // ui32Val = HWREG(GPIO_PORTN_BASE + GPIO_O_PCTL); ui32Val &= 0xFFFF00FF; ui32Val |= 0x0000FF00; HWREG(GPIO_PORTN_BASE + GPIO_O_PCTL) = ui32Val; // // EPI0S00 ~ EPI0S03, EPI0S31 : K0 ~ 3, K5 // ui32Val = HWREG(GPIO_PORTK_BASE + GPIO_O_PCTL); ui32Val &= 0xFF0F0000; ui32Val |= 0x00F0FFFF; HWREG(GPIO_PORTK_BASE + GPIO_O_PCTL) = ui32Val;
Rather than use DRM, I think this example would be clearer to use a sequence of GPIOPinConfigure calls to set the EPI pin muxing. I noticed this when modifying the example to run on some different hardware, in which the required pin-muxing was different.