I am using a Stellaris Launchpad LM4F120XL. As I was learning about the hibernation feature I accidentally programmed the board with code that doesn't allow enough time to program the board before hibernating. So now I am unable to reprogram the board. I have tried using the LM Flash programmers unlock feature. I held the reset button as I powered it on and then tried to unlock. The LM Flash programmer was unable to connect to the device.
Is there anything I should be doing differently to get this to work? If not, is there anything else I should try?