Other Parts Discussed in Thread: TM4C123GH6PM, EK-TM4C123GXL
I’m using TM4C123GH6PM, Tiva Launch Pad EK-TM4C123GXL to be more specific.
I have a SPI Master sending me commands, so I should parse the command and act accordingly.
I configure my chip as SPI Slave
void Ssi0Setup(void)
{
// The SSI0 peripheral must be enabled for use.
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
// For this example SSI0 is used with PortA[5:2].
//SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
// Configure the pin muxing for SSI0 functions on port A2, A3, A4, and A5.
GPIOPinConfigure(GPIO_PA2_SSI0CLK);
GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinConfigure(GPIO_PA4_SSI0RX);
GPIOPinConfigure(GPIO_PA5_SSI0TX);
// Configure the GPIO settings for the SSI pins.This function also gives
GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 |
GPIO_PIN_2);
SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
SSI_MODE_SLAVE, 2000000, 8);
// Enable the SSI0 module.
SSIEnable(SSI0_BASE);
//enable interrupts
SSIIntEnable(SSI0_BASE, SSI_RXFF | SSI_RXTO | SSI_RXOR );
// Read any residual data from the SSI port. This makes sure the receive
// FIFOs are empty, so we don't read any unwanted junk.
while(SSIDataGetNonBlocking(SSI0_BASE, &ssi_data_rx[0]))
{
}
}
int main()
{
ClockSetup();
GpioSetup();
UartSetup();
Ssi0Setup();
//Enable processor interrupts.
ROM_IntMasterEnable();
//to see the chip alive
UARTSendStr("Endat test\r");
while(1)
{
if(ssi_int_flag)
{
ssi_int_flag = 0;
SSIDataGet(SSI0_BASE, &ssi_data_rx[0]);
// Since we are using 8-bit data, mask off the MSB.
ssi_data_rx[0] &= 0x00FF;
ssi_command = (ssi_data_rx[0] & 0x00CF);
switch(ssi_command)
{
case ENC_SND_POS_VAL:
UARTSendStr("Encoder send position values\r");
Blink(1);
break;
case ENC_SEL_MEM_ARE:
UARTSendStr("Selection of memory area\r");
Blink(2);
break;
case ENC_REC_PARAM:
UARTSendStr("Encoder receive parameter\r");
Blink(3);
break;
case ENC_SND_PARAM:
UARTSendStr("Encoder send parameter\r");
Blink(4);
break;
case ENC_REC_RST:
UARTSendStr("Encoder receive reset\r");
Blink(5);
break;
default:
UARTSendStr("Invalid command\r");
break;
}
//clear FIFO
while(SSIDataGetNonBlocking(SSI0_BASE, &ssi_data_rx[0]))
{ }
}
}
}
//Interrupt for SSI0
void SSI0_ISR(void)
{
UARTSendStr("SSI Int\r"); //for debug
uint32_t int_status;
//Get the interrrupt status.
int_status = ROM_SSIIntStatus(SSI0_BASE, true);
// Clear the asserted interrupts.
ROM_SSIIntClear(SSI0_BASE, int_status);
if(int_status==SSI_RXFF)
{
ssi_int_flag = 1;
}
}
I get no interrupt also i see valid signal on SSI0Rx and SSI0CLK lines.