This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Improved UARTprintf

I was in need of an octal display feature in UARTprintf and in implementing that I put in several new features and improvements and couple of bug fixes (I think).

Here is some actual output showing features and examples  :

Features :

%% = '%' displays %
%c = 'C' character value
%d = '4779' decimal value
%i = '4779' decimal value identical to %d
%o = '11253' octal value
%p = '101D' address value (identical to %X
%P = '&0000101D' address value
%s = 'Abcdef' string
%u = '4294962517' unsigned decimal value
%x = '12ab' hexadecimal value
%X = '12AB' hexadecimal value
%q = '%q' unimplemented formats 

Modifiers :

These are inserted between the % and the format character.
They are recognized in the following order :

+        for signed numbers, always show a sign.
- or ^   align left or center for numbers and strings.
0        for numbers, left padding uses 0 instead of space.
#        decimal width for display field.

Examples and tests:

%+-05%= '%'%d = '123'

%-d = '123'
%5d = ' 123'
%-5d = '123 '
%05d = '00123'
%-05d = '00123'
%+5d = ' +123'
%+-5d = '+123 '
%+05d = '+0123'
%+-05d= '+0123'
%2d = '123'
%-2d = '123'
%02d = '123'
%-02d = '123'
%+2d = '+123'
%+-2d = '+123'
%+02d = '+123'
%+-02d= '+123'

%d = '-123'
%-d = '-123'
%5d = ' -123'
%-5d = '-123 '
%05d = '-0123'
%-05d = '-0123'
%+5d = ' -123'
%+-5d = '-123 '
%+05d = '-0123'
%+-05d= '-0123'
%2d = '-123'
%-2d = '-123'
%02d = '-123'
%-02d = '-123'
%+2d = '-123'
%+-2d = '-123'
%+02d = '-123'
%+-02d= '-123'

%s = 'Abcdef'
%10s = ' Abcdef'
%-10s = 'Abcdef '
%^10s = ' Abcdef '
%^11s = ' Abcdef '
%^11s = ' Abcdef '

%p = '101D'
&%08p = '&0000101D'
%P = '&0000101D'

And here my version of UARTprintf :


//***************************************************************************** // //! A simple UART based vprintf function supporting \%c, \%d, \%o, \%p, \%s, \%u, //! \%x, and \%X. //! //! \param pcString is the format string. //! \param vaArgP is a variable argument list pointer whose content will depend //! upon the format string passed in \e pcString. //! //! This function is very similar to the C library <tt>vprintf()</tt> function. //! All of its output will be sent to the UART. Only the following formatting //! characters are supported: //! //! - \%c to print a character //! - \%d or \%i to print number as a decimal value //! - \%o to print a number as an octal value //! - \%s to print a string //! - \%u to print an unsigned number as a decimal value //! - \%x to print an unsigned number as a hexadecimal value using lower case letters //! - \%X to print an unsigned number as a hexadecimal value using upper case letters //! - \%p to print a pointer value as a hexadecimal value //! - \%P to print a pointer value as a hexadecimal value "%P" is same as "&%p08X" //! - \%\% to print out a \% character //! //! For \%d, \%i, an optional ``\+'' character at immediately after the \% causes //! positive numbers to be displayed with a ``\+'' sign. //! For \%s, \%d, \%i, \%u, \%p, \%o, \%x, and \%X, an optional number may precede //! the format character, specifying the minimum number of characters to use for //! that value; if preceded by a 0 on numeric conversions then the extra characters //! will be filled with zeros instead of spaces. //! For example, ``\%8d'' will use eight characters to print the decimal value with //! spaces added to reach eight; ``\%08d'' will use eight characters as well but //! will add zeroes instead of spaces. //! //! The type of the arguments in the variable arguments list must match the //! requirements of the format string. For example, if an integer was passed //! where a string was expected, an error of some kind will most likely occur. //! //! \return None. // //***************************************************************************** void UARTvprintf (const char *pcString, va_list vaArgP) { uint32_t ui32Idx, ui32Value, ui32Base; int iWidth; const char *pcStr; char *pcDigits, cFill, // fill character is space or zero (for numerics) cAlign, // may be 0 for left, '-' for right or '^' for centered cSign; // + : always show sign, 0: show only minus sign. ASSERT (pcString != 0); // Check the format string not null pointer while (*pcString) { // Loop while there are more characters in the string. // Find the first non-% character, or the end of the string. for (ui32Idx = 0; (pcString[ui32Idx] && (pcString[ui32Idx] != '%')); ui32Idx++) ; if (ui32Idx) { UARTwrite (pcString, ui32Idx); // Write this portion of the string. pcString += ui32Idx; // Skip the portion of the string that was written. } if (!*pcString) break; pcStr = ++pcString; // Skip the %. // Set initial values : cSign = *pcString == '+' ? *pcString++ : 0; // sign character cAlign = (*pcString == '-' || *pcString == '^') ? *pcString++ : '+'; // alignment cFill = *pcString == '0' ? *pcString++ : ' '; // fill character pcDigits = (char *) g_pchex; // Lower case hex digits ui32Base = 0; // no numeric display radix for (iWidth = 0; *pcString >= '0' && *pcString <= '9';) // Read width number iWidth = iWidth * 10 + (*pcString++ - '0'); switch (*pcString++) { // Handle the format command character. case 'c': // %c ui32Value = va_arg (vaArgP, uint32_t); // Get the value from the varargs. UARTwrite ((char *)&ui32Value, 1); // Print out the character. break; // End of %c command case 's': // %s pcStr = va_arg (vaArgP, char *); // Get the string pointer from the varargs. for (ui32Idx = 0; pcStr[ui32Idx]; ui32Idx++) // Determine length of the string. ; if ((cAlign != '-') && (iWidth > ui32Idx)) { uint32_t sp = iWidth - ui32Idx; if (cAlign == '^') sp >>= 1; iWidth -= sp; while (sp) sp -= UARTwrite (" ", sp > 4 ? 5 : sp); // fill left } UARTwrite (pcStr, ui32Idx); // Write the string. iWidth -= ui32Idx; while (iWidth > 0) iWidth -= UARTwrite (" ", iWidth > 4 ? 5 : iWidth); // fill right break; // End of %s command //--------------------- Numeric conversions -------------------------------------- case 'o': // Octal unsigned number if (!ui32Base) // real %o since base not set ui32Base = 8; // Set the base to 8. case 'P': if (!ui32Base) { // real %P since no base not set iWidth = 9; // Set width to 8 digits + sign cFill = '0'; // fill with 0 cSign = '&'; // Use sign to prefix with '&' ui32Base = 16; // base 16 pcDigits = (char *)g_pcHEX; } case 'u': // Handle the %u command. if (!ui32Base) // real %u since base not set ui32Base = 10; // Set the base to 10. case 'X': case 'p': if (!ui32Base) // real %X since base not set pcDigits = (char *)g_pcHEX; case 'x': if (!ui32Base) // real %x/%p since base not set ui32Base = 16; // All numerics fall through to here to perform the conversion, // ui32Base is the conversion base. case 'd': case 'i': ui32Value = va_arg (vaArgP, uint32_t); // Get the value from the varargs. if (!ui32Base ) { // real %d/%i since base not set if ((int32_t)ui32Value < 0) { // Negative value ui32Value = -(int32_t)ui32Value; // Make the value positive. cSign = '-'; // Indicate that the value is negative. } ui32Base = 10; // Set the base to 10. } // Determine the number of digits in the string version of the value. for (ui32Idx = 1; (((ui32Idx * ui32Base) <= ui32Value) && (((ui32Idx * ui32Base) / ui32Base) == ui32Idx)); ui32Idx *= ui32Base) iWidth -= 1; iWidth -= 1 + !!cSign; // Sign present, reduce count of padding characters. // If a sign is present and the value is padded with zeros, // then place the sign before the padding. if (cSign && (cFill == '0')) { UARTwrite (&cSign, 1); // write the sign character cSign = 0; // and turn off sign } if (cAlign != '-' || cFill == '0') // Pad to left while (iWidth > 0) iWidth -= UARTwrite (&cFill, 1); // write the fill character if (cSign) // If a sign is present UARTwrite (&cSign, 1); // ... write it // Write out the digits for (; ui32Idx; ui32Idx /= ui32Base) UARTwrite (pcDigits + ((ui32Value / ui32Idx) % ui32Base), 1); while (iWidth > 0) iWidth -= UARTwrite (" ", iWidth > 4 ? 5 : iWidth); // fill right break; // End of numeric conversions default: // Handle all other commands. pcString = pcStr; // Restore pointer case '%': UARTwrite ("%", 1); // Simply write a single %. break; // End of unknown commands } } }