Other Parts Discussed in Thread: TM4C123GH6PM, CC3100, CC3100SDK
Hi,
I want to try mDNS on my Tiva TM4C123GH6PM with CC3100 custom board. After installing CCS6.0.1, I create a Hello World CCS project, taking TI v5.1.6 as compiler. Then I drag and drop C:\ti\CC3100SDK_1.0.0\cc3100-sdk\examples\mdns\main.c to the project (with "Copy" option selected) and delete hello.c.
In Build Settings of the project, Build - ARM- Include options, I add to the upper window the following 3 paths: "C:\ti\CC3100SDK_1.0.0\cc3100-sdk\simplelink\include", "C:\ti\CC3100SDK_1.0.0\cc3100-sdk\examples\common" and "C:\ti\CC3100SDK_1.0.0\cc3100-sdk\platform\tiva-c-launchpad". I can then pass the build phase easily but when linking, the below error appears:
**** Build of configuration Debug for project mDNS **** "c:\\ti\\ccsv6\\utils\\bin\\gmake" -k all 'Building file: ../main.c' 'Invoking: ARM Compiler' "c:/ti/ccsv6/tools/compiler/arm_5.1.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="c:/ti/ccsv6/tools/compiler/arm_5.1.6/include" --include_path="C:/ti/CC3100SDK_1.0.0/cc3100-sdk/simplelink/include" --include_path="C:/ti/CC3100SDK_1.0.0/cc3100-sdk/examples/common" --include_path="C:/ti/CC3100SDK_1.0.0/cc3100-sdk/platform/tiva-c-launchpad" -g --gcc --define=ccs="ccs" --define=PART_TM4C123GH6PM --display_error_number --diag_warning=225 --diag_wrap=off --preproc_with_compile --preproc_dependency="main.pp" "../main.c" 'Finished building: ../main.c' ' ' 'Building file: ../tm4c123gh6pm_startup_ccs.c' 'Invoking: ARM Compiler' "c:/ti/ccsv6/tools/compiler/arm_5.1.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="c:/ti/ccsv6/tools/compiler/arm_5.1.6/include" --include_path="C:/ti/CC3100SDK_1.0.0/cc3100-sdk/simplelink/include" --include_path="C:/ti/CC3100SDK_1.0.0/cc3100-sdk/examples/common" --include_path="C:/ti/CC3100SDK_1.0.0/cc3100-sdk/platform/tiva-c-launchpad" -g --gcc --define=ccs="ccs" --define=PART_TM4C123GH6PM --display_error_number --diag_warning=225 --diag_wrap=off --preproc_with_compile --preproc_dependency="tm4c123gh6pm_startup_ccs.pp" "../tm4c123gh6pm_startup_ccs.c" 'Finished building: ../tm4c123gh6pm_startup_ccs.c' ' ' 'Building target: mDNS.out' 'Invoking: ARM Linker' "c:/ti/ccsv6/tools/compiler/arm_5.1.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -g --gcc --define=ccs="ccs" --define=PART_TM4C123GH6PM --display_error_number --diag_warning=225 --diag_wrap=off -z -m"mDNS.map" --heap_size=0 --stack_size=512 -i"c:/ti/ccsv6/tools/compiler/arm_5.1.6/lib" -i"c:/ti/ccsv6/tools/compiler/arm_5.1.6/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="mDNS_linkInfo.xml" --rom_model -o "mDNS.out" "./main.obj" "./tm4c123gh6pm_startup_ccs.obj" "../tm4c123gh6pm.cmd" -l"libc.a" <Linking> undefined first referenced symbol in file --------- ---------------- CLI_Configure ./main.obj CLI_Write ./main.obj _SlNonOsMainLoopTask ./main.obj initClk ./main.obj sl_DevGet ./main.obj sl_NetAppDnsGetHostByService ./main.obj sl_NetAppMDNSRegisterService ./main.obj sl_NetAppMDNSUnRegisterService ./main.obj sl_NetCfgSet ./main.obj sl_Start ./main.obj sl_Stop ./main.obj sl_WlanConnect ./main.obj sl_WlanDisconnect ./main.obj sl_WlanPolicySet ./main.obj sl_WlanProfileDel ./main.obj sl_WlanRxFilterSet ./main.obj sl_WlanSet ./main.obj sl_WlanSetMode ./main.obj stopWDT ./main.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "mDNS.out" not built >> Compilation failure gmake: *** [mDNS.out] Error 1 gmake: Target `all' not remade because of errors. **** Build Finished ****
These link errors are due to the inability to find the source code of the listed functions.
AFAIK, CLI_Configure function is in cli_uart.c under "C:\ti\CC3100SDK_1.0.0\cc3100-sdk\platform\tiva-c-launchpad" which was already included above but it seems the compiler (TI v5.1.6) just ignores. I tried to add that path to library search path in Project settings - Build - ARM Linker - File Search Path but that does not help.
My questions:
1) C:\ti\CC3100SDK_1.0.0\cc3100-sdk\examples\mdns\main.c is the right source code to experiment mDNS service? If not, could you show me the correct link or mDNS sample project?
2) How to make the compiler (TI v5.1.6) "understand" functions in C source files such as cli_uart.c
Thanks in advance,