I am attempting to use the USB DFU functionality in the ROM on a EK-TM4C1294XL.
After erasing flash and connecting the USB, the device enumerates correctly as "Stellaris Device Firmware Upgrade" and device manager says the driver is installed and it is working correctly. But, when I run Uniflash setup for the Tiva/LM USB DFU Interface, and click "Display DFU devices" no devices are found.
Any suggestions?