This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

internal temperature sensor TM4C1294



Hello,

1. I read values from internal temperature sensor with ADC. In data sheet I found formula for temperature calculation:

TEMP = 147.5 - ((75 * (VREFP - VREFN) × ADCCODE) / 4096)

My VREFP = 3.3V and VREFN = 0V, I multiplied all 10 and in code formula looks:

final_result = (double)(1475 - 75 * 33 * sample / 40960);

It gives me value too high, about 55 degree Celsius.

When I use formula from older project that use Stellaris processor: 

final_result = (double)((1475 * 4096 - 75 * 33 * sample) / 40960);

it gives me more logical value, about 35 degree Celsius.

What is wrong with formula that I obtained from data sheet of Tiva?

2. I work also with couple another external temperature sensors in the same way like internal temperature sensor.

I paid attention on that when I connect external sensor I see that measured temperature of internal sensor of Tiva increases by 4 degrees.

Why it happens?

3. The temperature measurement occurs every 2 sec by interrupt from timer. Within these short intervals temperature can vary by several degrees. The measurement is carried out in a laboratory where there is no abrupt temperature jumps. Other sensors doesn't have these jumps. Is it proper work for internal temperature sensor?

Example of current code:

	uint32_t sequence;
	uint32_t channel;
	uint32_t sample;
	double	 final_result;
			
	// configure the ADC sequence
	MAP_ADCSequenceConfigure(ADC0_BASE, sequence, ADC_TRIGGER_PROCESSOR, 0);
	MAP_ADCSequenceStepConfigure(ADC0_BASE, sequence, 0, channel | ADC_CTL_IE | ADC_CTL_END);
	MAP_ADCSequenceEnable(ADC0_BASE, sequence);
	MAP_ADCIntClear(ADC0_BASE, sequence);

	MAP_ADCProcessorTrigger(ADC0_BASE, sequence);
	// Wait for conversion to be completed.
	while(!MAP_ADCIntStatus(ADC0_BASE, sequence, false)) {}

	MAP_ADCSequenceDataGet(ADC0_BASE, sequence, &sample);
	
	final_result = (double)((1475 * 4096 - (75 * 33 * sample)) / 40960);

Regards,

Sergey