Hi,
I want to build a custom PCB on which I can use the BlackHawk ARM JTAG probe ( USB100v2-ARM). If i got it correctly the Pin out for this JTAG can be found here:
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0499b/BEHEIHCE.html
So this is the Jtag pin out schematic I got so Far:
Pin 2 is unconnected, Rpullow1 = Rpulllow2 = 1k. I Don't know what to do with Pin 11 (RTCK) and Pin 3 (nTRST)
My Jtag TDI/TDO/TCK/TMS are pull-up with 1k. The reset pin is pull-down with a 1k.