Hi
My customer found CAN would jump in transmit interruption continuously when update to SDK 2.1.3.156, no this problem if back to SDK 2.1.2.111.
Compare the code, the difference is line1113 at TivaWare_C_Series-2.1.2.111\driverlib\can.c
SDK 2.1.3.156:HWREG(ui32Base + CAN_O_IF1CMSK) |= CAN_IF1CMSK_CLRINTPND;
SDk 2.1.2.111:HWREG(ui32Base + CAN_O_IF1CMSK) = CAN_IF1CMSK_CLRINTPND;
Is it a SW bug?
2.Can we use 100 meter length network cable to running 500kbps speed? Thanks.