Part Number: DRV8353R
Hi,
I was hoping to seek clarification on the return path of GLx. It appears that the return path will be SPx when using a shunt resistor. If this is true, then I assume that best practice would be to make the SPx trace as thick as the GLx trace to accommodate the possible 2A current flow. This would mean that one would not use relatively thinner differential traces that are common for current sensing since SPx is also used for current sensing?
Respectfully,
Lucas