Other Parts Discussed in Thread: TLC555
Hi all,
we realized a board to test the DRV8306 controlling a 24V BLDC motor (see attached diagram).
I have a TLC555 which generates a 0-99% PWM and everything works fine: the motor run and we are able to control the speed by moving the potentiometer R92.
But, when I apply a 0 to DVDD pulse step on the PWM pin (i.e: PWM at 100%) by closing pin 3 and 4 of SH10 jumper the motor won't run (it seems stuck): sometimes I can hear a little gear movement, but then it doesn't run.
I have already tried to tie VDS and IDRIVE pins to VDD but nothing changed.
Can you help me?
Thank you in advance,