Other Parts Discussed in Thread: DRV8305
Couple questions on the Wake pin of the DRV8305 that are not addressed in the datasheet (that I can find):
- Is there a pull-up or pull-down on the WAKE pin?
- What is the timing required after pulling WAKE high? Is it 10ms like PVDD rising above UVLO?
- The customer wants to use the WAKE pin to put the part to sleep. Can this be done by writing sleep to register 9 and then pulling WAKE low later when sleep is desired or do they need to pull WAKE low then write SLEEP to register 9?
Thanks,
Greg