Other Parts Discussed in Thread: DRV8320, DRV8301
Hi,
I have a motor control board with the DRV8320R as a gate driver and I see some ringing, which seems to be proportional to the applied motor phase current.
The ringing looks like the following, where the yellow probe is the supply voltage and the blue probe the SHC (motorphase):
So there is a overshoot of around 5V at 20A. I use the following MOSFETs: BSC0702LSATMA1 (https://www.mouser.ch/datasheet/2/196/Infineon_BSC0702LS_DataSheet-1770891.pdf)
with 11nC gate capacity. The DRV8320 setting for the smart gate current is 60mA/120mA, so this should be low enough.
Is this too much overshoot? From the datasheet it seems, the driver will turn off and set a fault, when the difference from VCC and SHX is more than 7V?
It is also seen on the ground line:
So might it be only a measurement error, since the GND is up from the current?