This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8908-Q1: Passive OLD mode control

Genius 17355 points
Part Number: DRV8908-Q1

Hello,

 

My customer is evaluating DRV8908-Q1 and are going to use passive open load detection.

 

According to the datasheet, POLD is enabled by setting HBX_POLD_EN in OLD_CTRL_5,  POLD_EN in CONCIG_CTRL and HBX_HS(or LS)_EN in OP_CTRL_1/2/3.

Then they are asking whether it is OK to disable and enable by just clearing and setting HBX_POLD_EN in OLD_CTRL_5 while remaining HBX_HS(LS)_EN is enabled.

I mean they want to switch to/from POLD mode directly from/to usual HS(or LS) ON by just changing HBX_POLD_EN bit.

Is it acceptable? In this case, can POLD_EN in CONFIG_CTRL  be always ON?

 

Regards,

Oba