Other Parts Discussed in Thread: DRV8332,
Hi
DRV8312 and DRV8332 are designed so that if 12V is supplied only for G VDD and VDD, current will leak to P VDD, isn't it?
I'm not sure about the internal circuit of the IC, but I want to prevent current from flowing to the OUT_A and OUT_B lines while supplying 12V.
Under this condition, I thought that it would be possible to prevent current from flowing by supplying 0V to P VDD. Is my perception correct?
(It is assumed that the equipment is on standby, not the motor is operating.)
Best regards
Naoki