Hi sir,
I would like to consult your product "DRV2667EVM-CT"
If I want to use it in Piezo actuator.
Can be achieve controlled vibration ?
In my impression, we consider the case that two objects are connected by Piezon actuator,
and the vibration of one side is transmitted through Piezon actuator,
it is thought that the vibration is absorbed in the piezo actuator by the vibration of the opposite phase with the input vibration.
Is this control possible?
Thanks.