This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
When customer evaluating DRV8844, they asks whether continuous motor drive output current can reach 3A, if with good heatsink natural cooling? since on datasheet the max is 2.5A, but don't know the thermal condition
Best regards
Gene
Hi Gene,
The 2.5A continuous current rating is the abs max rating. So we don't guarantee that the device will function normally if the current is pushed above 2.5-A. You may be able to push the current up to 3-A with good heatsink and cooling but the device may malfunction due to the high current.