Other Parts Discussed in Thread: DRV120
Hi,
I am looking for a functional substitute for DRV110 , which has available stock.
Could you please provide me any viable suggestions?
Thank you!
Regards,
Alberto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alberto,
Unless you can provide additional information to your desired system functionality, my suggestion is to search for solenoid drivers specific to your application here: Solenoid Drivers | Overview | Motor Drivers | TI.com
Thanks,
Kevin
Hi Kevin,
this is to drive a solenoid , 600mA hit (50ms), 200mA hold.
25khz (above audible).
Has to be HW settable.
Regards,
Alberto
Hi Alberto,
Please confirm parameters for a DRV110 application:
T_KEEP = 50ms
I_PEAK = 600mA
I_HOLD = 200mA
F_PWM = 25kHz
Could you explain why you are looking for a substitute?
Thanks,
Kevin
Hi Kevin,
yes the parameters are correct.
They need a substitute because there is no availability for DRV110.
Please let me know what an equivalent solution using something with AVAILABLE stock is.
Thank you!
Best regards,
Alberto
Hi Alberto,
Oh I see, 8-pin DRV110 is out of stock. 8-pin DRV120 has stock, however, this wouldn't fit your application since this configuration locks I_HOLD at 50mA .
Both 14-pin DRV110/DRV120 are stocked, both will fit your desired application and more, based on the specified parameters.
Otherwise, I recommend you search for other solenoid drivers within ti.com. Hope this helps.
Thanks,
Kevin