Other Parts Discussed in Thread: DRV8316, DRV8316-Q1
Hi
Our customer now need to find a driver IC ,an external mosfet drives a BLDC, the motor power is about 50W. I search the DRV8343-Q1 has 3 current senses(which could do the FOC algorithm while it is also OK without current sense amplifier) Do we have a size-smaller chioce? I think 8316 has a built-in half bridge, and the current is not enough. The demand is that because the normal working current of the motor is about 5A, the stall current is below 20A and we need an automotive device recommendation. In addition, I see DRV8316 is a catalog and automotive level device, does itself support AEC-Q100 or only DRV8316Q1 support AEC-Q100 but DRV8316 not? Thank you very much!