Hi Experts,
Could you help me answering the following questions from a customer?
Question_A:
What are the possible disadvantages of the operating mode "MODE = level 4" (Split HS and LS Solenoid Control) with the DRV8705-H. Are there any, or in other words are all diagnostics, protection functions, slew rate setting (IMODE), etc. available and usable as in the other modes?
What is not or only limited available in "MODE = level 4" (features, diagnostics, protection function, ...)?
Why is "solenoid" explicitly mentioned?
Is with "MODE =level 4" not also a DC motor with PWM controllable (10-16A).
Question_B:
The voltage at 'DRAIN' (IC-Pin_28) is used as a "reference" for short circuit/overcurrent detection per Uds of the HS-FET's by the DRV. +Ubat is directly connected to IC-Pin_28 (DRAIN).
I have seen a resistor (100R) at this point in a (different) application.
What is the " judgement" on the part of TI here?
Is a resistor "allowed" here? If so, what would be the maximum value?
Best regards,
Simon