Hi Team,
Customer would to know whether the two outputs of current detection are detected separately when driving a DC brushed motor? Or is it enough to just detect one AD together?
Thanks,
Annie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Annie,
The device has 2 iPropi pins. One pin monitors current on the high-side of one FET and the other pin monitors current on the other high-side FET (connected on other side of motor). For bi-directional control, only one current monitor will register current depending on forward or reverse control.
Please see section 7.3.1.3 in the datasheet:
7.3.1.3 Internal Current Sense and Current Regulation
Regards,
Ryan