Part Number: DRV8876
Other Parts Discussed in Thread: DRV8874
It seems that only peak current is mentioned in the datasheet.
I couldn`t find a guaranteed current specification.
1. Is it possible up to 2A for continuous current?
In 60℃ environment, DRV8876 heat is too high, and it does not operate normally.
2. If I use the DRV8874, will it work properly in a 60℃ environment?
please answer these two questions.