Hi Team
Our customer bought DRV8106S-Q1EVM then he followed the instructions in the User's Guide. After installing the version 0.5.1, the GUI asked to install the update and when he did the board didn't worked. The GUI recognized the port number as shown in the screenshot below, however, it shows that no EVM is connected. The status LED is blinking and the fault LED is on. Is there an error with the firmware?
Regards,
Danilo