Hello...
I just want to confirm this....Do I need to put a pull down on the EN pin of the above subject? After looking at the datasheet and the typ. application ckt it appears that the device has an internal 2M ohm pulldown and if I drive this signal hi I will be enabled.
Also can you confirm if I need pulldowns on the IN/TRIG as well?
Thank you
Steve