This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN1B044PWPR : Does the motor need to stop completely before it can start again?

Other Parts Discussed in Thread: DRV8308

Hi,

Does the device need to be completely stopped after it has been ENABLE low and before it can be restarted?

Also, if this "motor must stop completely before it can be restarted" specification, is there a workaround for this?

* Because the customer-requested specifications require the motor to be restarted before it is completely stopped.

* For example, with the DRV8308, it seems that the motor needs to be stopped completely before restarting, but this is a problem.

Regards,