Hi Team,
We would like to ask your help regarding the customer's inquiry below regarding DRV110AQPWRQ1.
Driving a heavy solenoid for a new industrial contactor rated at 11 Ohms and 141 MilliHenry Inductance. Using the T.I. Evaluation (EVM) module for testing, that module will not adjust the Holding current very much. On the T.I. Evaluation module, we changed the shunt resistor from 1.0 Ohms to 0.5 Ohms. Copied this same change to our prototype circuit board. Set the EVM C3 capacitor to 1µF and that does produce our 0.1 Second "Keep" time just fine. Adjusting the "Peak" resistor to 78 KOhms, our peak value of 1.5 Amperes comes in just fine. Our heavy solenoid pulls in just fine. Our Holding current, as measured on the 36 Volt power supply reads 40 Milliamperes or much too low. We want nearly three times this value. Adjusting the "Hold" resistor up and down, we can reach 70 Milliamperes but no higher with numerous resistor value changes. While the power supply reads 40 Milliamperes, the peak volts across the 0.5 Ohm shunt resistor reads 0.125 Volts with a 10% duty cycle or 0.25 amperes. We are using the R7 & C1 low-pass filter on our prototype, same as the EVM module uses. We have tried various shunt values from 0.2 Ohms to 0.41 Ohms also but not a 1.0 Ohm. BTW, we use a separate and fixed 12 VDC supply for the EVM and prototype units. We cannot program the Holding current to achieve a higher value even on the EVM module. According to the T.I. Drive Parameter program, we should be in a working range for the shunt.
Thank you for your support!
Regards,
Danilo