This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8703-Q1: Alternates

Part Number: DRV8703-Q1

We are using the DRV8703QRHBTQ1. The lead times are ...

I'm looking for alternative options:

1. Anywhere to get a couple hundred of these?

2. Is there a better/similar part that has availability of a couple hundred?

3. Can I add current regulation to a part such as DRV835x? And what are the circuit recommendations?

4. New pre production parts are an option.

Some vague requirements: 28 volt nominal power supply, 4 amp peak current. Drives a brush type motor, bidirectional with PWM.

Any help is appreciated.