This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10975EVM: Unable to drive the motor

Part Number: DRV10975EVM
Other Parts Discussed in Thread: DRV10975

Hi Team,

The driver board is 24V power supply. Two brushless motors are used for testing, the rated voltages are 7.4V and 24V, and the motor cannot continue to run after two or three revolutions. Customer would like to know what parameters need to be set in detail?

Thanks,

Annie