This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV110EVM: DRV module :peak current issues

Part Number: DRV110EVM
Other Parts Discussed in Thread: DRV110

Hi,

     We had issues  peak ripple current with DRV110EVM Evaluation module.

Please waveform details as below.

Case 1: Peak to peak ripple current while valve on to off & off to on condition  .

Case 2: Peak to peak ripple current while valve on-off  condition 

 .

  Setting with DREV110EM module:

1. Hold current set to 50mA @ 200K POT R5

2.Peak current set to 220mA @ 270k POT R4.

3.PWM frequency set to 200k @ 20KHZ POT R6.

observation: Valve current peak to peak ripple is more during valve on condition ,off-on /on-off condition.

Please let me know any clarification required further .

and do the needful as soon as possible.

Regards,

Moorthi sekar

ph:7019605896/8971634695

Mail id:moorthi_sekar@baxter.com