Hi experts, I have a question of DRV8343S_Q1.
When I test DRV8343S-Q1EVM, I find the start performances of the high side MOSFETs and the low side MOSFETs are different. There are some oscillations in the Vgs waveform of the high side MOSFETs, when it goes into the miller platform. However there is no oscillation in the Vgs waveforms of the low side MOSFETs. And when I increase the IDRIVE, the oscillation on the high side MOSFETs will be worse.
I find the Power supplies for the high side drivers and low side drivers are different. For the high side drivers, the supplies are charge pumps. And for low side drivers, the supplies are linear regulators.
Is power supply related to the Vgs waveform? Is this the root course for this phenomenon?